AXIS#.FBUS.VL.CMD

Description

This command allows reading the velocity command set by fieldbus when in certain fieldbus modes.

Fieldbus Applicable Modes
EtherCAT Profile Velocity and Cyclic Synchronous Velocity
CANopen Profile Velocity and Cyclic Synchronous Velocity
PROFINET Velocity target when using NIST_A/B signals
EtherNet/IP Velocity target when using command types 7 (jog) and 8 (velocity setpoint) while AXIS#.OPMODE is velocity

  • This command can only be written while enabled and be reset when the drive changes operation modes. The commanded value is only in affect when AXIS#.CMDSOURCE is set to fieldbus.

Versions

Action Version Notes
Implemented 02-04-06-000

 

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s

See Velocity Units.

Range

Depends on units. See Velocity Range.

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

Fieldbus variants: AKD2G-SPP, AKD2G-SPE, AKD2G-SPC